The L Series jaw coupling provides positive engagement resulting in great strength because of the large area of contact of the elastomer "spider" center member with the interlocking jaws. This 3 piece coupling (two hubs and one spider) provides "fail safe" operations, as it will continue to run, even if the elastomer "spider" fails. The link below goes to all L line coupling components. While the range of coupling sizes is very large, sizes L035 and L050 (the two smallest sizes) are to be considered for motion control.