All Product Types > INDUSTRIAL MOTION PRODUCTS > Couplings & Power Transmission Parts Catalog > Disc Couplings > SXC Type (Close Coupled)  
 

SXC Type (Close Coupled)

    The SXC Type is the close coupled variation of the SX Type coupling. The SXC is similar to the SX coupling in that the disc packs are attached when the coupling is installed. In the close coupled units, the hubs are turned inward and are mounted inside the spacer. Note that with the hubs inside the spacer, the maximum bore allowed in the hub will be decreased. The SXC couplings can be used with one or both hubs turned outward to allow the coupling to accommodate different shaft separations.
    Note: The SXC Type uses the same disc pack kits and spacers as the SX Type.

    Click on a Product to view details.



    SXC-6 Type Closed Coupled Industrial Coupling Hubs w/ Keyway - Metric


    SXC-6 Type Closed Coupled Industrial Coupling Hubs w/ Keyway - Metric


    SXC-6 Type Closed Coupled Industrial Coupling Hubs w/ Keyway - Metric

    SXC-6 Type Hubs - Rough Stock Bore

    (9)

    SXC-6 Type Hubs with Keyway - Inch (Imperial) Bores

    (5)

    SXC-6 Type Hubs with Keyway - Metric Bores

    (2)


    Disc Pack - 6 Bolt


    Disc Pack - 6 Bolt


    Disc Pack - 6 Bolt

    Disc Pack Kits - Standard

    (17)

    Disc Pack Kits - High Speed

    (11)

    Disc Pack Kits - Overload

    (15)