|
Batch CAD Cart (0)
▾
Horizontal Split Cover Grid Couplings
horizontal-split-cover-grid-couplings
Grid Coupling Tapered Components - Cover/Grid Assembly, Horizontal Style - Imperial(17)
Grid Coupling Tapered Components - Cover/Grid Assembly, Horizontal Style - Metric(17)
Grid Coupling Tapered Components - Seal Kit, Horizontal Style - Metric(17)
Grid Coupling Straight Components - Hub Pilot w/ Puller Hole, Horizontal Style - Metric(5)
Grid Coupling Straight Components - Cover/Grid Assembly, Horizontal Style - Imperial(2)
Grid Coupling Straight Components - Cover/Grid Assembly, Horizontal Style - Metric(2)
Grid Coupling Straight Components - Seal Kit, Horizontal Style - Metric(2)
Grid Coupling Tapered Components - Cover, Horizontal Style - Imperial(17)
Grid Coupling Tapered Components - Cover, Horizontal Style - Metric(17)
Grid Coupling Tapered Components - Cover Hardware, Horizontal Style - Imperial(6)
Grid Coupling Tapered Components - Cover Hardware, Horizontal Style - Metric(7)
Grid Coupling Straight Components - Cover, Horizontal Style - Imperial(2)
Grid Coupling Straight Components - Cover, Horizontal Style - Metric
Grid Coupling Straight Components - Cover Hardware, Horizontal Style - Imperial
Grid Coupling Straight Components - Cover Hardware, Horizontal Style - Metric
Grid Coupling Hubs - Inch Bore / Keyway, Horizontal & Vertical Cover Style(173)
Lovejoy’s grid style coupling design has demonstrated its ability to dampen vibration by as much as 30% and can cushion shock loads that could cause damage to both the driving and driven equipment. The tapered grid spring design absorbs impact energy by spreading the energy out over the full length of the grid spring thus reducing the magnitude of the torque spikes. The Lovejoy design uses a curved hub tooth profile which creates a progressive contact with the flexible grid spring as the application torque increases. This feature provides a more effective and efficient transmission of power in properly aligned couplings. Lovejoy’s versatile design of industry standard hubs and grid springs for both horizontal and vertical cover styles allow Lovejoy couplings to be interchangeable with other industry standard grid couplings and components. Proper grid coupling installation and maintenance can add to a longer coupling life. Grid spring replacement is simple and can be performed at a fraction of the cost and time of a complete coupling.
Grid Coupling Hubs - Metric Bore / Keyway(59)
Lovejoy’s grid style coupling design has demonstrated its ability to dampen vibration by as much as 30% and can cushion shock loads that could cause damage to both the driving and driven equipment. The tapered grid spring design absorbs impact energy by spreading the energy out over the full length of the grid spring thus reducing the magnitude of the torque spikes. The Lovejoy design uses a curved hub tooth profile which creates a progressive contact with the flexible grid spring as the application torque increases. This feature provides a more effective and efficient transmission of power in properly aligned couplings. Lovejoy’s versatile design of industry standard hubs and grid springs for both horizontal and vertical cover styles allow Lovejoy couplings to be interchangeable with other industry standard grid couplings and components. Proper grid coupling installation and maintenance can add to a longer coupling life. Grid spring replacement is simple and can be performed at a fraction of the cost and time of a complete coupling.
Grid Coupling Taper Lock Bushing Hubs - Metric(20)
Grid Coupling Tapered Components - Grid Only - Metric(16)
Grid Coupling Straight Components - Grid Only - Metric(3)
|
Site Map | Privacy Statement | Terms & Conditions | Careers | Contact Us Follow us on:
© 2016 The Timken Company.
© 2016 The Timken Company.